AXIS#.VL.ARZF1 TO AXIS#.VL.ARZF4

Description

AXIS#.VL.ARZF1 sets the natural frequency of the zero (numerator) of AR filter 1. This value is FZ in the approximate transfer function of the filter:

ARx(s) = [s²/(2πFZ)² +s/(QZ2πFZ) + 1]/ [s²/(2πFP)² +s/(QP2πFP) + 1]

The following block diagram describes the AR filter function; note that AR1 and AR2 are in the forward path, while AR3 and AR4 are applied to feedback:

AR1, AR2, AR3, and AR4 are used in velocity and position mode, but are disabled in torque mode.

Discrete time transfer function (applies to all AR filters)

The velocity loop compensation is actually implemented as a digital discrete time system function on the DSP. The continuous time transfer function is converted to the discrete time domain by a backward Euler mapping:

s ≈ (1-z-1)/t, where t = 62.5 µs

The poles are prewarped to FP and the zeros are prewarped to FZ.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Hz

Range

5 to 5,000 Hz

Default Value

AXIS#.VL.ARZF1: 5000 Hz

VLARZF2 to VLARZF4: 500 Hz

Data Type

Float
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
AXIS1.VL.ARZF1

5011h

18h

Unsigned32

-

1000:1

Read/Write

No

AXIS1.VL.ARZF2

5011h

19h

Unsigned32

-

1000:1

Read/Write

No

AXIS1.VL.ARZF3

5011h

1ah

Unsigned32

-

1000:1

Read/Write

No

AXIS1.VL.ARZF4

5011h

1bh

Unsigned32

-

1000:1

Read/Write

No

AXIS2.VL.ARZF1

5111h

18h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.VL.ARZF2

5111h

19h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.VL.ARZF3

5111h

1ah

Unsigned32

-

1000:1

Read/Write

No

AXIS2.VL.ARZF4

5111h

1bh

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.ARZF1

6012

177C

Signed32

Read/Write

-

AXIS2.VL.ARZF1

71548

1177

Signed32

Read/Write

-

AXIS1.VL.ARZF2

6013

177D

Signed32

Read/Write

-

AXIS2.VL.ARZF2

71549

1177

Signed32

Read/Write

-

AXIS1.VL.ARZF3

6014

177E

Signed32

Read/Write

-

AXIS2.VL.ARZF3

71550

1177

Signed32

Read/Write

-

AXIS1.VL.ARZF4

6015

177F

Signed32

Read/Write

-

AXIS2.VL.ARZF4

71551

1177

Signed32

Read/Write

-

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.ARZF1

6012

Float

Read/Write

-

AXIS#.VL.ARZF2

6013

Float

Read/Write

-

AXIS#.VL.ARZF3

6014

Float

Read/Write

-

AXIS#.VL.ARZF4

6015

Float

Read/Write

-